A can manufacturer had a problem in that they were needing to constantly replace vacuum hoses on the printing rollers for the canning line. This resulted in a loss of production of 1,900 cans per minute whilst the maintenance crew carried out the work.
Over the course of a year, this was having a major impact on production through 780 minutes of downtime.

A Rubix Insite™ Manager & Local Technical Specialist came up with the idea of using a convoluted stainless steel hose with an increased bend radius and greater flexibility. The new product is easier to fit and has performed extremely well with no reported failures.

780 minutes downtime per annum was saved at a production rate of 1,900 cans per minute. This resulted in 1,482.000 extra cans per annum being produced. At a cost of £30.00 per 1,000 cans, a huge saving was achieved.
Saving €55,575