Intra Domain Refining Policy Solutions
Solution 1: Individual Tables with IP Address White Lists
Requirements:
- Multiple user tables in the database
- Users are able to access a specific user table only if the user is connecting from an IP address approved for that table
- The set of approved IP addresses for a specific table must be administered through the SQL client interface by a specific administrative user connecting from a specific IP address (127.0.0.1)
Environment of Solution:
- Administrative table iplists created with columns user-table-name (string) and ip-address (string)
- Each row in iplists specifies the name of a user table (user-table-name column) in the database and an IP address (ip-address column) that may be used to connect to that table
- A row in iplists indicates users may access the table specified by name in user-table-name from the IP address specified by ip-address
- The administrative user has a user name of ipadmin
- User tables created and populated as desired
Security Policy of Solution:
- DAC permissions given to user ipadmin on table iplists for all operations
- DAC permissions given to basic users on user tables as desired
- All objects and sessions are at label Unclassified
- SPM policy called IPlists targeting all operations and assigned to table iplists. Rules are evaluated in order and the policy evaluates to Permit immediately if a rule evaluates to Permit; otherwise, it evaluates to Deny
- The IPlists policy contains the following rules:
- Rule1: If user name is ipadmin and subject's IP address context attribute is 127.0.0.1 then Permit
- Rule2: Deny
- SPM policy called UserTab targeting all operations. Rules are evaluated in order and the policy evaluates to Permit immediately if a rule evaluates to Permit; otherwise, it evaluates to Deny
- The UserTab policy contains the following variable definition:
- Extract all values of the ip-address column of table iplists where the user-table-name column value is equal to the resource attribute table-name (this will create a multi-valued container with all values of ip-address whose corresponding user-table column value is equal to the name of the table currently being operated upon)
- The UserTab policy contains the following rules:
- Rule1: If the current operation is of type open then Permit
- Rule2: If subject's IP address context attribute is within the multi-valued container specified by the variable definition then Permit
- Rule3: Deny
- The UserTab policy is configured with a scope covering the subtree and assigned to the database (this will cover all existing objects in the database and new objects as they are created)
Behavior of Solution:
Any user who accesses a table from a client host with a corresponding user-table-name / ip-address entry in the iplists table will succeed. All users who access a table from a client host without a corresponding user-table-name / ip-address entry in the iplists table will fail. Access to table iplists from client IP addresses other than 127.0.0.1 or from users other than ipadmin will fail. User ipadmin will be able to perform any operation on table iplists from client host 127.0.0.1. As updates to the iplists table occur the effects upon the security policy behavior will be immediate and transactionally controlled.
Solution 2: Row Access Restricted to Row Creator
Requirements:
- Single user table
- Table rows may be accessed only by the user that created the row
Environment of Solution:
- A table named tab created with desired columns and a column named creator (string)
Security Policy of Solution:
- DAC permissions given to users on table tab as desired
- All objects and sessions are at label Unclassified
- SPM policy called UserTabInsert targeting an operation of insert and always evaluates to Permit
- The UserTabInsert policy contains the following obligation:
- Obligation 1: On Permit set the value of the creator column to the value of the subject-name context attribute
- SPM policy called UserTabAllOthers targeting all operations except insert. Rules are evaluated in order and the policy evaluates to Permit immediately if a rule evaluates to Permit; otherwise, it evaluates to Deny
- The UserTabAllOthers policy contains the following rules:
- Rule1: If the current operation is of type open then Permit
- Rule2: If operation is not update and the subject-name context attribute is equal to the owner column value then Permit
- Rule3: If operation is update and the column owner is not being updated and the subject-name context attribute is equal to the owner column value then Permit
- Rule4: Deny
- SPM security policy set is assigned to table tab containing policies UserTabInsert and UserTabAllOthers. Policies are evaluated in order and the policy set evaluates to Permit immediately if a policy evaluates to Permit; otherwise, it evaluates to Deny
Behavior of Solution:
All rows in the tab table will have the user name of the inserter as the value of the owner column. All attempts to update the owner column will fail. All row based operations, other than update of the owner column, will succeed only if the current user name is equal to the value of the owner column of the row being operated upon. All select operations on the tab table will have all rows with owner column values that are not equal to the current user name filtered out of the result set.