You are hereSecurity Policy Enforcement / Trusted RUBIX Security Architecture

Trusted RUBIX Security Architecture


  

The security policy architecture of the Trusted RUBIX DBMS is shown in the following diagram and indicates the following:

  • the location of policy access checks relative to the SQL Engine and DBMS Kernel is represented by the position of the box labeled with the security policy name. Policy access checks are executed over operations and objects in the DBMS module directly below it. The DAC policy operates over SQL Engine operations and objects while all other policies operate over DBMS Kernel operations and objects. A policy being above another policy implies that it is evaluated after the other policy;
  • the values each policy uses to calculate its security decision are enumerated in the rectangular box to the right of the box labeled with the security policy name;
  • the basic characteristics of each security policy's rules are listed under the security policy name;
  • note that only security policies that operate directly on DBMS objects are shown (the RBAC policy is not shown).

 

Trusted RUBIX Security Archectecture